AXIS#.SAFEPARAM.SSR_#.FAULTREACTION

Description

Indicates the safety function activated when Safe Speed Range (SSR) is faulted. The parameter allows one of the following values:

Value Description

1

STO

2

SS1 Instance 1

3

SS2 Instance 1

 

Context

For complete SSR information refer to SSR (Safe Speed Range).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

N/A

Range

1, 2, 3

Default Value

1 (STO)

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SSR_1.FAULTREACTION

3161h

0bh

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SSR_2.FAULTREACTION

3162h

0bh

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SSR_3.FAULTREACTION

3163h

0bh

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSR_1.FAULTREACTION

3261h

0bh

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSR_2.FAULTREACTION

3262h

0bh

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSR_3.FAULTREACTION

3263h

0bh

Unsigned8

-

-

Read/Write

No